Why is the air you're breathing at home so important?
We consume about 1 kg of food and 2 kg of water daily, but did you know we inhale around 15 kg of air in the same period? While we can survive weeks without food and days without water, we can only go minutes without air.
We spend 90% of our time indoors, but unfortunately the quality of the air we breathe at home can be up to five times worse than it is outdoors
Of course outdoor sources like pollen, and general air pollution can add to the problem, but some of the culprits such as pollutants from the dust or allergens can be found around the home. Even daily activities such as dust released from the cleaning or odours from cooking can influence the quality of the air we breathe. The finer the particles, the more dangerous they are to our health. Fine Particulate Matter (PM2.5) defined as particles with diameter equal to or less than 2.5 microns are so small that they remain invisible, giving us a false sense of safety. But with the right filtration system you can reduce the impact of these pollutants from the air.
Six reasons to choose an air purifier
An air purifier is a useful addition to every home, but it’s particularly recommended for people with allergies, asthma and respiratory problems. Households with young children, pregnant women or older people are especially vulnerable to indoor air pollution.
How does a Daikin air purifier work?
Daikin air purifiers can help fight against respiratory diseases, pollen and other seasonal allergies. A three-step approach reduces fine, harmful particles:
Why choose a Daikin air purifier?
- Testing
- Advanced filtration
- Comfort
We have been tested for respiratory viruses and allergies
Daikin has been trusted and tested by renowned institutions.
Daikin MC55W can remove more than 99.9% of respiratory viruses in 2.5 minutes, as tested by the Institut Pasteur de Lille. (Read test results in the footnote below). Daikin MC55w was given the allergy seal of approval by British Allergy Foundation (BAF) and is approved allergy-friendly by European Centre for Allergy Research (ECARF).
A multi-stage filtration for best results
Our air purifiers feature a complete filtration system, with three stages of filtration. The first stage is a pre-filter that helps to capture and remove large particles such as dust, pet hair, and lint. The second stage is an electrostatic HEPA filter that captures and removes small particles such as allergens, dust mites, and smoke. The third stage is a deodorizing filter that helps to reduce odours in the air.
Our electrostatic HEPA filters do not depend on the mesh size but catch pollutants through their static charge.
Unlike a regular filter, it doesn’t require a smaller mesh size, which would be prone to clogging. This means it only needs replacing every ten years.
Purifying air made easy
Our plug-and-play units include 'auto-mode', allowing the purifier to constantly monitor and clean the air as needed, and automatically switch off when not required. Additionally, you’ll enjoy healthier air in peace, thanks to their whisper-quiet operation, with noise levels as low as 19dBA.
The different types of air purifiers
Air purifier without humidifier
View all the features on the discreet and functional MC55W Air Purifier
View Air Purification Technology
Give the gift of comfort with allregen reducing air purifiers and Air Conditioners that have built in HEPA filters
Discover
Support
More Daikin
Utility links